Part Number: TMS320F280034
Tool/software:
Properly added 2 pull up resistors for GPIO24 & 32 for flash mode operation.
But with the available CMD file, BEGIN address not consistant.
With BEGIN 80000, programmer give error.
With 88000 , programming. Running with debugger, but not after power up.
MEMORY
{
RAMM0 : origin = 0x00000128, length = 0x000002D8
RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
RAMLS01 : origin = 0x00008000, length = 0x00001000
RAMLS27 : origin = 0x00009000, length = 0x00003000
RAMGS01 : origin = 0x0000C000, length = 0x00002000
RAMGS23 : origin = 0x0000E000, length = 0x00001FF8
BOOTROM : origin = 0x003F8000, length = 0x00007FC0
SECURE_ROM : origin = 0x003F2000, length = 0x00006000
BEGIN : origin = 0x00088000, length = 0x00000002
RESET : origin = 0x003FFFC0, length = 0x00000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x088002, length = 0x000FFE /* on-chip Flash */
FLASH_BANK0_SEC1_12 : origin = 0x081000, length = 0x005000 /* on-chip Flash */
FLASH_BANK0_SEC1314 : origin = 0x086000, length = 0x005000 /* on-chip Flash */
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : > FLASH_BANK0_SEC1_12, ALIGN(8)
.cinit : > FLASH_BANK0_SEC1_12, ALIGN(8)
.switch : > FLASH_BANK0_SEC1_12, ALIGN(8)
.econst : > FLASH_BANK0_SEC1_12, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used */
Please help me with proper CMD file.