Part Number: TMS320F28335-Q1
Tool/software:
Hello E2E Experts,
Good day.
We are using P/N: TMS320F28335ZJZQ in our data acquisition project, I have two queries mentioned below
1) In Technical Reference Manual, it mentioned that if 'TALK' Bit of SPICTL Register is disabled transmission data, Default state of SIMO pin will be in high impedance
But If TALK' Bit of SPICTL Register is enabled, then no transmission data is written to SPITXBUF Register & there is no previous transmission data in SPITXBUF Register, What will be default state of SIMO pin? clearly
2) I have same above query in McBSP-A&B configured as SPI. What is the default state of SIMO pin is enabled for transmission if there is no transmission data written & no previous transmission data?
I appreciate a clear explanations.
Regards,
TICSC