Part Number: TMS320F28P550SG
Tool/software:
Hi Team,
My customer is upgrade F28075 to F28P55, they have the same layout, use the same analog device, but F28P55 will damage(VDD short to GND) at 4KV surge, F28075 work well.
There are the test result, at 4KV surge
When use ISO-485, it will damage F28P55.
When use non-ISO-485, F28P55 not damage.

They re-layout PCB and add some TVS, but still don't pass 4KV surge test.
In new board, if they remove DCDC do 4KV surge test, it will not damage F28P55.

Could you give us some advice? Thanks!
Best Regards,
Zane