Part Number: TMS320F280025C
Tool/software:
Hello.
I am using the EPWM module but use only one side (A or B
only).
So I do not configure the action qualifier for the unused pins, how should I connect them?
Is it ok to leave it unconnected?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025C
Tool/software:
Hello.
I am using the EPWM module but use only one side (A or B
only).
So I do not configure the action qualifier for the unused pins, how should I connect them?
Is it ok to leave it unconnected?
Hiroki,
It is okay to leave it unconnected/floating.
In case you want to use that GPIO on channel B for something else the do not assign that GPIO to channel B. You follow the procedure below with code snippet: To use only one ePWM channel A without channel B in C2000, you need to configure the ePWM module to operate in a single channel mode. Each ePWM module in C2000 has two output channels, A and B, but they can be configured independently. Here are the steps to configure channel A without using channel B:
// Configure ePWM1 channel A EPwm1Regs.TBPRD = 1000; // Set period EPwm1Regs.CMPA.bit.CMPA = 500; // Set duty cycle to 50% EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // Set output on EPWM1A at CTR=0 EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Clear output on EPWM1A at CTR=CMPA // Leave ePWM1 channel B disabled EPwm1Regs.AQCTLB.bit.ZRO = AQ_NO_ACTION; // No action on EPWM1B EPwm1Regs.AQCTLB.bit.CBU = AQ_NO_ACTION;