Part Number: LAUNCHXL-F280049C
Tool/software:
Hi,
We are running our motor with F280049C and boostXL-DRV 8323 with the following MATLAB example.
the motor runs fine in open and close loop at PWM_frequency = 20 Khz. we would like to see the current harmonics at 32 and 40 kHz. However when we change the frequency to higher than 24 Khz , the actual speed (from sensor) will become half the command speed. This behavior cannot be observed in Simulink scopes as it seems like the speed is following the command properly (but in reality it is half). It does work for 24Khz but nothing above that. We were wondering if you can help us with this problem.
another question that we have is that it seems when we set the PWM_frequency = 20 Khz, the switching frequency is double this value (40Khz) while the current sampling frequency remain at 20Khz. why is that?
Thanks for your help in advance.