Part Number: TMS320F2800157
Tool/software:
Hello,
I am working on RAM ECC parity test. I have ITRAP on PIERAMParityTest function when index is 1.
After first iteration "RPC 0x3FFD2C Return Program Counter [Core]" goes this value which is not on the ram or flash range. After index set to 1 when returning from "STL_RAM_testRAMLogic" function, cpu generates ITRAP. Data on PIE_RAM_TEST_ADDR is 0x000BB155 and original is 0x0009B157
I tried "sdl_ex_ram_ecc_parity_test" example, it is works fine on the same MCU.
I have added "STL_RAM_" prefix on the functions. The functions are same with "sdl_ex_ram_ecc_parity_test" example
// Using the I2CB interrupt (8.3) for testing here, but you may select others
#define STL_RAM_PIE_RAM_TEST_INT INT_I2CB
#define STL_RAM_PIE_RAM_TEST_PIEIFR_REG (PIECTRL_BASE + PIE_O_IFR8)
#define STL_RAM_PIE_RAM_TEST_PIEIFR_BIT (PIE_IFR8_INTX3)
#define STL_RAM_PIE_RAM_TEST_ACK INTERRUPT_ACK_GROUP8
#define STL_RAM_PIE_RAM_TEST_ADDR 0x00000DB4UL
uint16_t w_test_STA_TEST_RAM_ECC_PARITY(bool injectError)
{
(void)injectError;
uint16_t returnVal;
uint16_t failCount;
// Clear all the NMI and RAM error status flags.
MemCfg_clearCorrErrorStatus(MEMCFG_CERR_CPUREAD);
MemCfg_clearCorrErrorInterruptStatus(MEMCFG_UCERR_CPUREAD);
MemCfg_clearUncorrErrorStatus(MEMCFG_UCERR_CPUREAD);
SysCtl_clearAllNMIFlags();
SysCtl_clearInterruptStatus(0xFFFFFFFFU);
// Configure the correctable error interrupt threshold.
MemCfg_setCorrErrorThreshold(1U);
// Plug the NMI and RAM correctable error ISRs.
Interrupt_register(INT_NMI, &STL_RAM_nmiISR);
Interrupt_register(INT_SYS_ERR, &STL_RAM_corrErrorISR);
Interrupt_enable(INT_SYS_ERR);
SysCtl_setInterruptStatusMask(STL_RAM_MASK_ALL_BUT_RAM_ERR);
// Plug a routine to handle a PIE Vector Table parity error
EALLOW;
HWREG(CPUSYS_BASE + SYSCTL_O_PIEVERRADDR) = (uint32_t) &STL_RAM_pieVectErrorHandler;
EDIS;
// Enabling the NMI global interrupt (typically already enabled by boot ROM
// or GEL file).
SysCtl_enableNMIGlobalInterrupt();
// Enable RAM correctable error interrupt.
MemCfg_enableCorrErrorInterrupt(MEMCFG_CERR_CPUREAD);
// Enable Global Interrupt (INTM) and Real Time interrupt (DBGM).
EINT;
ERTM;
// Test parity functionality by injecting an error in parity RAM.
failCount = STL_RAM_runParityTest();
// Test parity functionality by injecting an error in PIE RAM.
failCount += STL_RAM_runPIERAMParityTest();
// Test ECC functionality by injecting a few correctable errors in m0Data_ECCParity.
failCount += STL_RAM_runCorrectableECCTest();
// Test ECC functionality by injecting an uncorrectable error in m0Data_ECCParity.
failCount += STL_RAM_runUncorrectableECCTest();
// Status of a successful handling of the RAM ECC/parity errors.
if(failCount != 0U)
{
//TEST FAIL: RAM ECC Parity Test!
returnVal = STA_TESTS_FAIL;
}
else
{
//TEST PASS: RAM ECC Parity Test!
returnVal = STA_TESTS_PASS;
}
return returnVal;
}