Part Number: TMS320F280037-Q1
Other Parts Discussed in Thread: TPS653860-Q1
Tool/software:
We are using this uC, whats the recommended PMIC? we need 5V, 3.3V and 3.3V. Vin from 6 to 36V. I have TPS653860-Q1 considered, but has too many output rails and C2000 is not in the list of compatible devices. Is there a compatible smaller/cheaper device with less outputs? Also, can any of the outputs be configured as wake to the micro when it receives the IGN signal?