Part Number: TMS320F28388D
Tool/software:
DEVICE_DELAY_US() library function not producing actual delay.
We are using CPU1 and CPU2 is disabled.
System clock is running at 200MHz produce from 20MHz external crystal.
#define DEVICE_OSCSRC_FREQ 20000000U
E.g..
we are trying to produce delay of 2500uS but actual produced delay is 4200uS.
Need help to get this resolve.
GPIO_writePin(RLY_CMD1_PIN,true);
GPIO_writePin(RLY_CMD2_PIN,true);
DEVICE_DELAY_US(2500); //2.5msec
GPIO_writePin(RLY_CMD1_PIN,false);
GPIO_writePin(RLY_CMD2_PIN,false);
Controller Module : TMS320F28388D
optimization Level is as suggested by optimizer assistant as follows.

I am generating 1ms timer interrupt and that is getting generated properly and can see 1ms periodicity.