This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: running out of memory

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Tool/software:

hi, 

I am getting this error message when i build my code in 28377D : ( I do have quite a bit of code )


<Linking>
"C:/ti/C2000Ware_5_04_00_00/device_support/f2837xd/common/cmd/2837xD_RAM_lnk_cpu1.cmd", line 81: error #10099-D:
program will not fit into available memory, or the section contains a call
site that requires a trampoline that can't be generated for this section.
placement with alignment/blocking fails for section ".cinit" size 0x2ec page
0. Available memory ranges:
RAMM0 size: 0x2dd unused: 0x2d9 max hole: 0x2d9
error #10010: errors encountered during linking;
"adc_soc_epwm_tempsensor_cpu01.out" not built

I remember there is a way to increase the memory size allocation. can I increase the memory allocation for RAMM0 ? 

thank you