Part Number: TMS320F28379S
Tool/software:
We are having a strange problem with one of our processors and I was looking to see if there is any guidance as to why this may be happening. A client found that at temperatures less than -15C, Comparator 5 would begin tripping without any input to the pin on the processor. The program on this processor has been verified, and no other device experiences this problem in the same configuration. We verified that there is no external noise on the input pin to this device, and the ADC result register tied to that comparator is not experiencing any jumps in value. The comparator status was verified via a Code Composer Studio debug session to be switching without any external input, only affected by cold temperature. Is this just a defective component?