Part Number: TMS320F280049C
Tool/software:
Hello.
Good day!
There is customer's issue ,could you help to clarify? Thank you so much.
Is the sampling channel for both current IB and IC , is it wrong?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C
Tool/software:
Hello.
Good day!
There is customer's issue ,could you help to clarify? Thank you so much.
Is the sampling channel for both current IB and IC , is it wrong?

Hi Alice,
Is the sampling channel for both current IB and IC , is it wrong?
For ISEN -B is sensed on ADC C Channel-7 & for ISEN -C is sensed on ADC B Channel-7, they both are different pins on device as well.
BR,
Nilesh
Hello Nilesh,
Thanks for your support.
There is some confusion, please help to clarify, thank you so much.
1) Do you mean each ADC has its own ADCIN channels?
There are 3 ADCs : ADCA ADCB ADCC , total 3*16 ADCIN channels ?
2) How to confirm the signal is assigned to the channel 7?
Hi Alice,

If we see for the Highligted section from the Snippet shared ISENB is connected to C7 throught PGA3 (Input pin of PGA3 is the I senB & PGA output would be routed to C7 in this case )
Similarly for the other case as well.
BR,
Nilesh
Yes below is correct, but we need to look at the muxing of these channels in datasheet to see which channels are mapped where.
1) Do you mean each ADC has its own ADCIN channels?
There are 3 ADCs : ADCA ADCB ADCC , total 3*16 ADCIN channels ?
Please note not all Channels of ADC are connected to device pins few are internal channels