Part Number: TMS320F28379D
Tool/software:
Hi Team ,
We are working with the Texas Instruments F28379D and the Embedded Coder Support Package for Texas Instruments C2000. The default f28379D.ccxml file is configured for the XDS100v2 debugger. However, we have manually configured Code Composer Studio (CCS) for the XDS110 debugger. After configuring the .ccxml file, we are encountering the following error. Please help us resolve this issue.
"No source available for "_system_post_cinit() at C:\Users\mputtaraju\Desktop\DC-DC-CONVERTER\MODELS\Toggle_GPIO\TOGGLE_LED_ert_rtw\CCS_Project\Debug\TOGGLE_LED.out:{3} 0x3fe493{4}"
"C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed."
"C28xx_CPU1: Trouble Reading Register SP: (Error -1156 @ 0x1) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 12.7.0.00105)"
Thanks,
Anusha.