This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28332: EN or IEC

Part Number: TMS320F28332

Tool/software:

Hello together, 

We require the following certificates for Australian approval: EN or IEC certificates for the products listed below.

TRUMPF SAP No.:

Manufacturer:

Type of Component

Manufacturer No.:

Standard

 

2244347

Texas Instruments

phy-CORE-AM335x

AM3359BZCZ

 

Keine Standards im Dokument vohanden

2300431

Texas Instruments

IC Micro Controller

TMS320F28374SPTPT

 

Keine Standards im Dokument vohanden

2833680

Texas Instruments

IC Micro Controller

TMS320F28375DPTPT

IEC 61508 up to SIL 3
IEC 60730 up to Class C
IEC 61508 up to SIL 2 certified

 

2006436

Texas Instruments

Transformer driver

ISO1176TDWR

DIN EN IEC 60747-17 (VDE 0884-17)
DIN EN 60112 (VDE 0303-11); IEC 60112
IEC 60664-1
IEC 61010-1

 

2354111

Texas Instruments

Transformer driver

ISO5852SDW

IEC 60950–1 and IEC 60601–1 End Equipment Standards
EN 61010-1 and EN60950-1
IEC 60112
IEC 60065
IEC 60601-1

 

2364007

Texas Instruments

Isolated Amplifier

AMC1301DWV

DIN EN IEC 60747-17 (VDE 0884-17)
IEC 62368-1
IEC 60112
IEC 60664-1
IEC 62368-1

 

 

 

 

 

 

 

 

 

Thank you and regards

Amina