This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Concerto: Peripheral Clock Speed

Hi TI Concerto team,

On the reference manual for the Concerto on page 316 it say that GPIO have the following:

-Fast toggle capable of a change every two clock cycles.

This mean  for example if I'm running at 100MHz on the M3, the GPIO can toggle as fast as 50MHz?

How can I achieve this?

I do some tests toggling the GPIO24 from inside of a infinite loop using the API: "GPIOPinWrite" the maximum toggling frecuency that I get was around 1.24MHz.

How can I improve the GPIO speed?

 

Regards,

Jorge Macias