Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Now, I'm considering using the TMS320F28377D and have two questions.
1) TMS320F28377D has CPU1 and CPU2. Do I need to create software for both?
(Should I create a separate CCS project for each?)
If I only use CPU1, is it possible that I don't need to create software for CPU2?
If I don't need to create it, how should I set the registers for CPU2?
If there are any documents or sample codes for register settings, please let me know.
Also, if it is necessary to create it, please let me know if there are any sample codes for setting the registers for CPU2.
2) If I want to use both CPU1 and CPU2 and use separate external buses (address bus, data bus),
(i.e., if I want CPU1 and CPU2 to control and access the bus independently and in parallel),
is such a setting possible? How should I set it up?
Please let me know if you have any sample code for such a case.
Also, is the GFP 176-pin package enough pins? Is it necessary to use a BGA package?
Regards,
T. Mori