This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: 97 pin output unexpected high level with power on.

Part Number: TMS320F28069

Tool/software:

Hi expert,

28069's pin 97 without any connection outputs a 3.3V high level for 30ms when powered on. How can this high level be avoided?

An 11k resistor is connected to ground externally, and the voltage level is 2V.

An 2k resistor is connected to ground externally, and the voltage level is 1.3V.

As below waveform, yellow is VDDIO, bule is pin97.

No connection:

Connect 11k:

Connect 2k:

Best Regards

Anka Zhang