Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I started a new development on LAUNCHXL-F28379D and strangely it seems that the clock is running at half of what is configured and expected. I double checked all clocks configurations but couldn't find any reason for that.
To verify this i loaded the CPU timers example (timer_ex1_cputimers) which configures the device to run 1sec interrupts and to increment counters on every interrupt. Monitoring the counters (with continuous refresh on the IDE) i can see that they are incrementing only every 2 seconds.
I am using CCS V20. Didn't change anything in the example code or in sysconfig. Just loaded it as is.
I wanted to output SYSCLK to a physical pin but XCLKOUT (GPIO73) is not available on LAUNCHXL-F28379D.
Any idea?
Thanks.
Timor