Part Number: TMS320F28P650DK
Tool/software:
I've been trying to utilized the DMA peripheral and encountered some problems.
I can see the addresses are configured accordingly but no data is transferred.
My goal: each ADCA1 event to trigger the DMA copy from the source address to the destination address.
I'm trying to copy 32bit uint32_t data type.
The data copy should be cyclic - once configured I don't want to reconfigure the DMA.
I can also tell the the ADCA1 event functions - I can get into the ISR function which is also triggered from the ADCA1 event.
This is my configuration for the DMA:

Is there something I'm missing? Does this configuration matches my needs?
Thanks,
Ariel