Part Number: TMS320F280039C
Other Parts Discussed in Thread: DESIGNDRIVE, C2000WARE, BOOSTXL-DRV8323RH, , TMS320F28069M, BOOSTXL-DRV8301, BOOSTXL-DRV8305EVM, BOOSTXL-DRV8323RS, BOOSTXL-3PHGANINV, MOTORWARE, LAUNCHXL-F28069M, DRV8305, DRV8301, LAUNCHXL-F28P55X, SYSCONFIG
Tool/software:
I need a microcontroller that allows me to:
- implement torque, speed and position control (obviously not all at the same time, I want to be able to try all three).
- sensored control (I will have an encoder and probably also a backup Hall sensor)
Can you advise me which microcontroller meets these two conditions?
If I understand correctly, while with the older generation (e.g. F28069M) you had about 21 project labs .. with the newer generation (F280039C) I have a single project with 4 debug levels, but I don't think there is a DEBUG_LEVEL that allows for position control .. or do I?
(not related to the question, but I had also read of someone who had tried (and succeeded) in 'converting/passing' one of the old project labs into the new microcontrollers... but it is not an easy thing to do and I don't remember there being an official guide)
Thank you.
Best regards