Other Parts Discussed in Thread: MOTORWARE
Tool/software:
Hi,
my project is using DSP TMS320F28388D + gate driver DRV8323RH (Gain current amplifer 10) + external mosfet to control BLDC motor by FOC algorithm.
My BLDC has rate speed is 8100RPM (Rate voltage 24VDC and current 4A), I use combination hall sensor and incremental encoder (2048 pulse per revolution) to calculate electric rotor angle for FOC.PWM frequency 12.5Khz, FOC current frequency = PWM frequency.
My problem is board can control motor in high speed range ( > 200RPM) very well,
but when control in low speed range (<100RPM) the quality very poor, motor runs not smooth (even no load). the torque I feel weak when run in low speed
Can some one point me some reason may make this issue or solution to improve quality control motor in low speed range?
brs,
longpt10