This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: The issue is related to merging two .out files into one hex file when the DSP is running.and it seems to be a rather complex.

Part Number: TMS320F28377D

Tool/software:

Hi  experts,I have encountered an issue, and now I will describe it in detail.

Test Environment
DSP Model: TMS320F28377D,Emulator: XDS100V3,CCS Version: 10.4.0
Problem Description 
After flashing the merged hex file (which is merged from boot.out and app.out), the instructions sent from the debugging interface fail to execute the corresponding program.
Procedure Description
1. Set the DSP Start address of CPU1 to 0x80000. After flashing the out file to CPU1, enter the debug run interface and send the command sCpu2ToCpu1Flag.uRigTestCode = 4 in the Expression interface. It is observed that the variable is set normally. Meanwhile, ePWM3.CMPA = 1262, and the corresponding pin 01 toggles.
1. Set the DSP Start address of CPU1 to 0x86000. After flashing the out file to CPU1, enter the debug run interface and send the command sCpu2ToCpu1Flag.uRigTestCode = 4 in the Expression interface. It is observed that the variable is set normally. Meanwhile, ePWM3.CMPA = 1262, and the corresponding pin 01 toggles.
Set Set the DSP Start address of CPU1 to 0x86000 and compile it into a hex file. After flashing the hex file to CPU1, enter the debug run interface and send the command sCpu2ToCpu1Flag.uRigTestCode = 4 in the Expression interface. The observed result is that ePWM3.CMPA = 0, and the corresponding pin 01 toggles.
Merge boot.out  and app.out into One hex Method:
1 Move the boot.out file to the output folder under the app directory.
2 enable hex file  generate
3  add hex cmd   hex2000 -i ../output/BOOT_BANK.out
Select the output file format.
Is the method of merging the hex files correct?  How should I go about identifying and resolving the abnormal operation issues?