Part Number: F29H85X-SOM-EVM
Tool/software:
I have configured EPWM in up down count mode, and programmed action qualifier such that EPWMXA output is high on CAD, CBD events . EPWMXA output low on CAU, CBU events. even CMPB is loaded with the zero it is reflecting on output. (in F28 controller, when CMPA, CMPB are loaded with zeros, they do not generating any actions). I need conformation on - " does Counter Compare modules generate events when they are loaded with the zeros in F29 controllers ".
Green - GPIO toggled on the TBCTR = 0 event.
Pink - EPWM output.
No one shot events or Sync In events, No Action qualifier configuration on TBCTR = 0 and TBCTR = TBPRD events.

Thanks, Regards,
Shashank B