Part Number: C2000WARE
Tool/software:
When I go to import a project from the C200Ware Motor Control SDK (v5.04.00), I get an error message which says
"See details below...
universal_servo_drive_f28p65x
Product C2000WARE v0.0 is not currently installed, and no compatible version is available. Please install this product or a compatible version."
However, I do have C2000ware (v5.04.00) installed in the same directory as the motor control SDK. I have been using c2000ware for over two weeks with no issue. I am using "workspace12" in CCS v12.8.