Part Number: TMS320F28388D
Tool/software:
I want to measure two motor phases current with shunt and then digitize with the Sigma Delta modulators AMC1306 and send back to the SDFM. Is there not an SDFM internal clock already? Do I have to feed an external clock in?
If I have to feed in an external clock, can I use a single ePWM pin on the F28388D to feed to two AMC1306 devices and also feed into SDFM? Do I need a buffer?
Thanks