This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SJ: F28P55: Is Single-ended 3.3-V External Clock require CL?

Part Number: TMS320F28P550SJ


Tool/software:

Hi Team,

My customer is using F28P55, signal-ended OSC 25MHz,  Passive crystal OSC will need calculate CL, does signal-ended OSC need think of the internal CL? 15pf can work?

Best Regards,

Zane

  • Hi Zane,

    CL is critical for external crystal as this will impact the accuracy and start up of the crystal.  In single-ended oscillator clocks, this is not critical but follow the oscillator manufacturer's specification just to be on the safe side.  Pin and pad capacitance of X1 is around 5pF for short PCB traces so seems like 10 to 15pF would be a good value to put in as CL to the oscillator's output.

    Regards,

    Joseph