This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: SCI_lockAutobaud in ex3_live_firmware_update example

Part Number: LAUNCHXL-F280049C

Tool/software:

Good day, 

In ex3_live_firmware_update for the LAUNCHXL-F280049C dev board there is an SCI_lockAutobaud(SCIA_BASE) in main. My question is how will the application code run when the system is powered on and not performing a live firmware update?  SCI_lockAutobaud function is a blocking function so when the board is powered on (and a firmware update is not being performed) the code would be blocked forever. 

Cheers, 

Scott