Part Number: TMS320F28P650DH
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello, expert. Currently, I am configuring SPI for the CCS-A project. Since this project does not have sisconfig, I have to configure it myself. Currently, the A project has successfully configured SCI and the sending and receiving are correct, which proves that the low-speed clock of the A project is correct. However, the configuration of SPI is incorrect at present.
I configured SPI correctly in Project B (verified successfully on the development board), but when I transferred the code from Project B to Project A for running, it didn't work properly. Could you please tell me what configuration I'm lacking and how to troubleshoot the issue?



void main(void)
{
//
// flush SCIA TX port by waiting while it is busy, driverlib.
//
// sciaFlush();
//
// initialize device and GPIO, driverlib.
//
Device_init();
Device_initGPIO();
//
// init interrupt and vectorTable, drivelib.
//
Interrupt_initModule();
Interrupt_initVectorTable();
//
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
//
// At 200MHz, execution wait-states for external oscillator is 4. Modify the
// wait-states when the system clock frequency is changed.
//
Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, 4);
//
// Pump access must be gained by the core using pump semaphore
//
EALLOW;
IPC_claimFlashSemaphore(IPC_FLASHSEM_OWNER_CPU1);
SysCtl_allocateFlashBank(SYSCTL_FLASH_BANK0, SYSCTL_CPUSEL_CPU1);
SysCtl_allocateFlashBank(SYSCTL_FLASH_BANK1, SYSCTL_CPUSEL_CPU1);
SysCtl_allocateFlashBank(SYSCTL_FLASH_BANK2, SYSCTL_CPUSEL_CPU1);
SysCtl_allocateFlashBank(SYSCTL_FLASH_BANK3, SYSCTL_CPUSEL_CPU1);
SysCtl_allocateFlashBank(SYSCTL_FLASH_BANK4, SYSCTL_CPUSEL_CPU1);
//Example_CallFlashAPI();
//
// initialize flash_sectors, fapi + driverlib
//
initFlashSectors();
EDIS;
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIA);
SysCtl_setLowSpeedClock(SYSCTL_LSPCLK_PRESCALE_4);
/*SCIA*/
GPIO_setControllerCore(DEVICE_GPIO_PIN_UARTARXDA, GPIO_CORE_CPU1);
GPIO_setPinConfig(DEVICE_GPIO_CFG_UARTARXDA);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_UARTARXDA, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(DEVICE_GPIO_PIN_UARTARXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_UARTARXDA, GPIO_QUAL_ASYNC);
//
// GPIO42 is the SCI Tx pin.
//
GPIO_setControllerCore(DEVICE_GPIO_PIN_UARTATXDA, GPIO_CORE_CPU1);
GPIO_setPinConfig(DEVICE_GPIO_CFG_UARTATXDA);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_UARTATXDA, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(DEVICE_GPIO_PIN_UARTATXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_UARTATXDA, GPIO_QUAL_ASYNC);
SCI_performSoftwareReset(SCIA_BASE);
initSCIA();
Interrupt_register(INT_SCIA_RX, INT_SCIA_BASE_RX_ISR);
Interrupt_register(INT_SCIA_TX, INT_SCIA_BASE_TX_ISR);
SCI_enableTxModule(SCIA_BASE);
SCI_enableRxModule(SCIA_BASE);
Interrupt_enable(INT_SCIA_RX);
Interrupt_enable(INT_SCIA_TX);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
// //uint32_t EntryAddr;
//
// //
// // parameter SCI_BOOT_ALT5 for GPIO28 (RX),29 (TX)
// //
// //EntryAddr = sciGetFunction(SCI_BOOT_ALT5);
// //return(EntryAddr);
//
memcpy(&RamfuncsLoadStart,&RamfuncsLoadEnd,RamfuncsRunStart);//将初始化Flash代码复制到RAM
//InitFlash();
memset(Byte_Data_Buf_RX,0,sizeof(Byte_Data_Buf_RX));
memset(Byte_Data_Buf_TX,0,sizeof(Byte_Data_Buf_TX));
memset(Word_Data_Buf_RX,0,sizeof(Word_Data_Buf_RX));
memset(Word_Data_Buf_TRX,0,sizeof(Word_Data_Buf_TRX));
Bytes_RX_D=0;
Bytes_cehsi=0;
// SysCtl_setPeripheralAccessControl(SYSCTL_ACCESS_SPIA,
// SYSCTL_ACCESS_CPUX, SYSCTL_ACCESS_FULL);
// SysCtl_setPeripheralAccessControl(SYSCTL_ACCESS_SPIA,
// SYSCTL_ACCESS_CLA1, SYSCTL_ACCESS_FULL);
// SysCtl_setPeripheralAccessControl(SYSCTL_ACCESS_SPIA,
// SYSCTL_ACCESS_DMA1, SYSCTL_ACCESS_FULL);
// SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIA);
#define FLASH_CS 61
GPIO_setPadConfig(FLASH_CS, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(FLASH_CS, GPIO_QUAL_SYNC);
GPIO_setDirectionMode(FLASH_CS, GPIO_DIR_MODE_OUT);
GPIO_setControllerCore(FLASH_CS, GPIO_CORE_CPU2);
//
// SPIA -> FLASH_SPIA Pinmux
//
//
// SPIA_PICO - GPIO Settings
//
#define GPIO_PIN_SPIA_PICO 16
#define FLASH_SPIA_SPIPICO_GPIO 16
#define FLASH_SPIA_SPIPICO_PIN_CONFIG GPIO_16_SPIA_PICO
//
// SPIA_POCI - GPIO Settings
//
#define GPIO_PIN_SPIA_POCI 17
#define FLASH_SPIA_SPIPOCI_GPIO 17
#define FLASH_SPIA_SPIPOCI_PIN_CONFIG GPIO_17_SPIA_POCI
//
// SPIA_CLK - GPIO Settings
//
#define GPIO_PIN_SPIA_CLK 18
#define FLASH_SPIA_SPICLK_GPIO 18
#define FLASH_SPIA_SPICLK_PIN_CONFIG GPIO_18_SPIA_CLK
//
// SPIA -> FLASH_SPIA Pinmux
//
GPIO_setPinConfig(FLASH_SPIA_SPIPICO_PIN_CONFIG);
GPIO_setPadConfig(FLASH_SPIA_SPIPICO_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(FLASH_SPIA_SPIPICO_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(FLASH_SPIA_SPIPOCI_PIN_CONFIG);
GPIO_setPadConfig(FLASH_SPIA_SPIPOCI_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(FLASH_SPIA_SPIPOCI_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(FLASH_SPIA_SPICLK_PIN_CONFIG);
GPIO_setPadConfig(FLASH_SPIA_SPICLK_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(FLASH_SPIA_SPICLK_GPIO, GPIO_QUAL_ASYNC);
FLASH_SPIA_init();
FlashEnableWrite();
FlashErase(0x20, 0);
FLASH_Byte_Write(Buffer,0,8);
FlashReadData(0, BufferA, 8, 0);
//
// //APP_UPDATA_CHK();//Example_CallFlashAPI
while(1)
{
}
}
}
void FLASH_SPIA_init(void)
{
//SPI_disableModule(FLASH_SPIA_BASE);
SPI_setConfig(FLASH_SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA1,
SPI_MODE_CONTROLLER, 11000000, 8);
SPI_setPTESignalPolarity(FLASH_SPIA_BASE, SPI_PTE_ACTIVE_LOW);
SPI_disableFIFO(FLASH_SPIA_BASE);
SPI_disableLoopback(FLASH_SPIA_BASE);
SPI_setEmulationMode(FLASH_SPIA_BASE, SPI_EMULATION_STOP_MIDWAY);
//SPI_enableModule(FLASH_SPIA_BASE);
}