Part Number: TMS320F28388S
Other Parts Discussed in Thread: C2000WARE
Tool/software:
[Background]
On CPU1, we call Device_bootCM(BOOTMODE_BOOT_TO_FLASH_SECTOR0) to trigger the boot process for the CM core.
On the CM side, we have only added the CM-related initialization function (CM_init()), and are otherwise using the default startup_ccs.c file provided by TI.
With this configuration, the CM core operates normally when running or restarting in a debug environment, but after a full power-off/on reset, the CM core does not boot up (as confirmed by external IO pin signals).
[Question]
What modifications or additional steps (e.g., source code changes, linker/compiler options, bootloader structure, etc.) are required to ensure that the CM core boots correctly after a power-on reset?
Also, is there an example project (including all project files and compiler options) available for download for this scenario?