Part Number: TMS320F28388D
Tool/software:
We have hardware and firmware working using the F28388D as our ESC for multiple EtherCAT nodes. However, we cannot not get the system to recognize our final EtherCAT node. This uses the same PHY as the other nodes and all connections to ESC0 are the same, the only difference between this node and the others is that the hardware connections to ESC1 have been removed. This includes ESC_RX1[...] ESC_TX1[...] and ESC_PHY1_LINK_STATUS1. We see communication between the PHY and the ESC but the node does not show up on a bus scan. Are there hardware requirements for ESC1 that need to be addressed to get this to work?