Part Number: TMDSCNCD28P65X
Tool/software:
(1)For DCL_PI_C4.asm provided by TI, does the assembly code have parameters for internal limits for both the integrator saturation and controller saturation? Please confirm. I see Umax,Umin but not Imax, Imin so wanted to confirm. Please suggest a way to incorporate the other if one of them it not included
Code can be found here:
(2) Also for ADCs, where would you recommend I trigger my EPWM SOC trigger from? This is important because I am designing a converter. Is it OK to trigger from when TBCTR= PRD or when a compare values is decrementing?
(3) Is it practical to trigger the ADC ISR interrupt and the ADC sample window from the same SOC. I have this set up but ADC ISR is much slower than I expect.
Regards.