This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Connectivity Manager configuration

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hello Sir,

I am using TMS320F28388D controller in one of my new project.

I have following query for this controller.

1. when i am using device support header from C:\ti\c2000\C2000Ware_5_03_00_00\device_support\f2838x\common\include in CM core for different module configuration then it is not supported.

2.For CM core configuration is only possible through driverlib_cm defined functions. How can i configure different modules by using f2838x_globalvariabledefs.C data sections as i am using for CPU-1 and CPU-2??

3.What should be the predefined symbol for CM_Core. Reference for Core-1 is as per below.

4.I am not able to use EALLOW and EDIS for CM Core.

5.Some of the .cmd file like f2838x_headers_nonBIOS_cpu1 and .asm file like f2838x_usdelay and f2838x_codestartbranch is not able to access in CM_Core.