Part Number: TMS320F280039C
Tool/software:
Hi Champs,
In datasheet 6.12.3.4.4 How to Choose a Crystal it says:
3. Check that the load capacitance requirement of the crystal manufacturer is within 6 pF and 12 pF per specifications for 20 MHz
So I think CL's recommended value is 6-12pF, and customer choose 10pF.
CL = [CL1]/2 + Cstray
If we think Cstray=5pF, CL1 will be 10pF, but datasheet require CL1's value is 12-24pF.
If CL chooses 6pF, the result calculated for CL1 is 2pF, still over-spec.
So how should we explain the conflict between the CL requirement of 6-12pF and the CL1 requirement of 12-24pF to the customer?
How should customers choose the value of CL/CL1/CL2?
Thanks!
Julia