This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: IEC 61508 FMEDA of TMS320F28388D in Cadence Midas Platform

Part Number: TMS320F28388D
Other Parts Discussed in Thread: MIDAS,

Tool/software:

Hellow,All,

I have a question regarding the TMS320F28388D package used in the Cadence Midas Platform。

As shown in the figure below, Cadence Midas Platform can use TMS320F28388D package,

but the file I got here only has PQFP package and no BGA package。

https://photos.google.com/photo/AF1QipNz8LZSl5qE36gfiVawa1fmjfpwnJn4ScAYIYQ_

I would like to ask the following questions:

01。 How can I obtain the FMEDA file for the TMS320F28388D BGA package?

02。 In the Cadence Midas platform, does the choice of TMS320F28388D package affect IEC 61508?

BR,

Vincent.