Part Number: TMS320F28388S
Tool/software:
Hi All,
The HRPWM operation is different from what I expected, so I want to know the cause.
The PWM settings are as follows.
・Count mode: Up-down count
・HRPWM application target: Falling edge
・HRPWM mode: Edge mode
・MEP scale factor: 64
・TBCLK: 100MHz (10ns)
・CMPAHR: 255 (8-bit left shift applied)
Given that the MEP scale factor is 64 and TBCLK is 10ns, I had expected that increasing the CMPAHR value by 1 would result in a delay of approximately 156ps,
and that the setting value of 255 would cause a delay of about 40ns.
However, when measured with an oscilloscope, the actual delay was only approximately 10ns, which is about one-fourth of the expected value.
Please explain the cause of this.
Is this behaviour acceptable?
Best Regards,
Ito