This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

New Thread for Firmware Upgrade Using Customized SCI Bootloader

Part Number: TMS320F28379D

Tool/software:

Hi Charles,

As mentioned in the thread linked below, we have initiated a new discussion regarding the firmware upgrade process using a customized SCI bootloader:

Link TI E2E Forum Thread – TMS320F28379D SCI Bootloader

Please refer to the above link for more detailed information.

If you need any further information or assistance, feel free to let us know.

Best regards,
Aditya

  • Hi Charles,

    Please find the below files for your refernce,

    Let me know if you need any further information.

    /*
    //###########################################################################
    // FILE:    flash_programming_cpu1_FLASH.cmd
    // TITLE:   Linker Command File For all F28X7x devices
    //###########################################################################
    // $TI Release: F2837xD Support Library v200 $
    // $Release Date: Tue Jun 21 13:00:02 CDT 2016 $
    // $Copyright: Copyright (C) 2013-2016 Texas Instruments Incorporated -
    //             http://www.ti.com/ ALL RIGHTS RESERVED $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    // The header linker files are found in <base>\F2837xD_headers\cmd
    // For BIOS applications add:      F28X7x_Headers_BIOS.cmd
    // For nonBIOS applications add:   F28X7x_Headers_nonBIOS.cmd
    ========================================================= */
    
    /* Define the memory block start/length for the F28X7x
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
       Notes:
             Memory blocks on F28M3Xx are uniform (ie same
             physical memory) in both PAGE 0 and PAGE 1.
             That is the same memory region should not be
             defined for both PAGE 0 and PAGE 1.
             Doing so will result in corruption of program
             and/or data.
    
             Contiguous SARAM memory blocks or flash sectors can be
             be combined if required to create a larger memory block.
    */
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
              /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
              /* BEGIN is used for the "boot to Flash" bootloader mode   */
    
      BEGIN           	: origin = 0x086000, length = 0x000002
       RAMM0           	: origin = 0x000122, length = 0x0002DE
       RAMD0           	: origin = 0x00B000, length = 0x000800
       RAMLS03          : origin = 0x008000, length = 0x002000
    /*	RAMLS1           : origin = 0x008800, length = 0x000800
        RAMLS2           : origin = 0x009000, length = 0x000800
        RAMLS3           : origin = 0x009800, length = 0x000800 */
       RAMLS4      		: origin = 0x00A000, length = 0x000800
       RAMGS14          : origin = 0x01A000, length = 0x001000
       RAMGS15          : origin = 0x01B000, length = 0x001000
       RESET           	: origin = 0x3FFFC0, length = 0x000002
    
    	/* Flash sectors */
       FLASHA           : origin = 0x080000, length = 0x002000	/* on-chip Flash */
       FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
       FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
       FLASHD           : origin = 0x086002, length = 0x001FFE	/* on-chip Flash */
       FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
       FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
       FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
       FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
       FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
       FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
       FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
       FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
       FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
       FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */
    
    PAGE 1 :   /* Data Memory */
             /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
    
        BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
    	RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
        RAMD1           : origin = 0x00B800, length = 0x000800
    
        RAMLS5      : origin = 0x00A800, length = 0x000800
    
    	RAMGS0          : origin = 0x00C000, length = 0x00B000
    	/*RAMGS1          : origin = 0x00D000, length = 0x001000*/
    	/*RAMGS2          : origin = 0x00E000, length = 0x001000*/
    	/*RAMGS3          : origin = 0x00F000, length = 0x001000
    	RAMGS4          : origin = 0x010000, length = 0x001000
    	RAMGS5          : origin = 0x011000, length = 0x001000
    	RAMGS6          : origin = 0x012000, length = 0x001000
    	RAMGS7          : origin = 0x013000, length = 0x001000
    	RAMGS8          : origin = 0x014000, length = 0x001000
    	RAMGS9          : origin = 0x015000, length = 0x001000
    	RAMGS10         : origin = 0x016000, length = 0x001000*/
    	RAMGS11         : origin = 0x017000, length = 0x001000
    	RAMGS12         : origin = 0x018000, length = 0x001000
    	RAMGS13         : origin = 0x019000, length = 0x001000
    
    
       CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
       CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
    }
    
    
    SECTIONS
    {
    
       /* Allocate program areas: */
       .cinit              : > FLASHD      PAGE = 0, ALIGN(8)
       .pinit              : > FLASHD,     PAGE = 0, ALIGN(8)
       .text               : >> FLASHD |FLASHE | FLASHF | FLASHG | FLASHH     PAGE = 0, ALIGN(8)
       codestart           : > BEGIN	PAGE = 0, ALIGN(8)
       
        GROUP
        {
            ramfuncs
            dclfuncs
            { -l F021_API_F2837xD_FPU32.lib}
         
        } LOAD = FLASHE,
          RUN  = RAMLS03, 
          LOAD_START(_RamfuncsLoadStart),
          LOAD_SIZE(_RamfuncsLoadSize),
          LOAD_END(_RamfuncsLoadEnd),
          RUN_START(_RamfuncsRunStart),
          RUN_SIZE(_RamfuncsRunSize),
          RUN_END(_RamfuncsRunEnd),
          PAGE = 0, ALIGN(8)
    
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : >> RAMLS5 | RAMGS0       PAGE = 1
       .esysmem            : > RAMLS5       PAGE = 1
    
       /* Initalized sections go in Flash */
       .econst             : >> FLASHE | FLASHF | FLASHG      PAGE = 0, ALIGN(8)
       .switch             : > FLASHE      PAGE = 0, ALIGN(8)
    
       .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       Filter_RegsFile     : > RAMGS0,	   PAGE = 1
    
       SHARERAMGS0		: > RAMGS0,		PAGE = 1
       SHARERAMGS1		: > RAMGS11,		PAGE = 1
    
       /* Flash Programming Buffer */
       BufferDataSection : > RAMD1, PAGE = 1, ALIGN(4)   
       
       /* The following section definitions are required when using the IPC API Drivers */ 
        GROUP : > CPU1TOCPU2RAM, PAGE = 1 
        {
            PUTBUFFER 
            PUTWRITEIDX 
            GETREADIDX 
        }
    
        GROUP : > CPU2TOCPU1RAM, PAGE = 1
        {
            GETBUFFER :    TYPE = DSECT
            GETWRITEIDX :  TYPE = DSECT
            PUTREADIDX :   TYPE = DSECT
        }  
    
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    
    
    
    

    MEMORY
    {
    PAGE 0 :  /* Program Memory */
              /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
       RAMM0           	: origin = 0x000122, length = 0x0002DE
       RAMD0           	: origin = 0x00B000, length = 0x000800
       RAMLS0          	: origin = 0x008000, length = 0x000800
       RAMLS1          	: origin = 0x008800, length = 0x000800
       RAMLS2      		: origin = 0x009000, length = 0x000800
       RAMLS3      		: origin = 0x009800, length = 0x000800
       RAMLS4      		: origin = 0x00A000, length = 0x000800
       RAMGS14          : origin = 0x01A000, length = 0x001000
       RAMGS15          : origin = 0x01B000, length = 0x001000
       RESET           	: origin = 0x3FFFC0, length = 0x000002
       
    
    #ifdef __TI_COMPILER_VERSION__
       #if __TI_COMPILER_VERSION__ >= 20012000
    GROUP {      /* GROUP memory ranges for crc/checksum of entire flash */
       #endif
    #endif
    
       /* BEGIN is used for the "boot to Flash" bootloader mode   */
       BEGIN           	: origin = 0x080000, length = 0x000002
    
       /* Flash sectors */
       FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
       FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
       FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
       FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
       FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
       FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
       FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
       FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
       FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
       FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
       FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
       FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
       FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
       FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */   
    #ifdef __TI_COMPILER_VERSION__
      #if __TI_COMPILER_VERSION__ >= 20012000
    }  crc(_table_name, algorithm=C28_CHECKSUM_16)
      #endif
    #endif
    
    PAGE 1 : /* Data Memory */
             /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
    
       BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAMD1           : origin = 0x00B800, length = 0x000800
    
       RAMLS5      : origin = 0x00A800, length = 0x000800
    
       RAMGS0      : origin = 0x00C000, length = 0x001000
       RAMGS1      : origin = 0x00D000, length = 0x001000
       RAMGS2      : origin = 0x00E000, length = 0x001000
       RAMGS3      : origin = 0x00F000, length = 0x001000
       RAMGS4      : origin = 0x010000, length = 0x001000
       RAMGS5      : origin = 0x011000, length = 0x001000
       RAMGS6      : origin = 0x012000, length = 0x001000
       RAMGS7      : origin = 0x013000, length = 0x001000
       RAMGS8      : origin = 0x014000, length = 0x001000
       RAMGS9      : origin = 0x015000, length = 0x001000
       RAMGS10     : origin = 0x016000, length = 0x001000
       RAMGS11     : origin = 0x017000, length = 0x001000
       RAMGS12     : origin = 0x018000, length = 0x001000
       RAMGS13     : origin = 0x019000, length = 0x001000
    
       
       CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
       CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
    }
    
    
    SECTIONS
    {
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0, ALIGN(8)
       .pinit              : > FLASHA,     PAGE = 0, ALIGN(8)
       .text               : >> FLASHA | FLASHB      PAGE = 0, ALIGN(8)
       codestart           : > BEGIN       PAGE = 0, ALIGN(8)
    
    #ifdef __TI_COMPILER_VERSION__
       #if __TI_COMPILER_VERSION__ >= 15009000
        .TI.ramfunc : {} LOAD = FLASHB,
                             RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_SIZE(_RamfuncsLoadSize),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             RUN_SIZE(_RamfuncsRunSize),
                             RUN_END(_RamfuncsRunEnd),
                             PAGE = 0, ALIGN(8)
       #else
       ramfuncs            : LOAD = FLASHB,
                             RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_SIZE(_RamfuncsLoadSize),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             RUN_SIZE(_RamfuncsRunSize),
                             RUN_END(_RamfuncsRunEnd),
                             PAGE = 0, ALIGN(8)
       #endif
    #endif
    						 
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1        PAGE = 1
       .ebss               : >> RAMLS5 | RAMGS0 | RAMGS1       PAGE = 1
       .esysmem            : > RAMLS5       PAGE = 1
    
       /* Initalized sections go in Flash */
       .econst             : >> FLASHB     PAGE = 0, ALIGN(8)
       .switch             : > FLASHA      PAGE = 0, ALIGN(8)
       
       .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       Filter_RegsFile     : > RAMGS0,	   PAGE = 1
       
       SHARERAMGS0		: > RAMGS0,		PAGE = 1
       SHARERAMGS1		: > RAMGS1,		PAGE = 1
       
       /* The following section definitions are required when using the IPC API Drivers */ 
        GROUP : > CPU1TOCPU2RAM, PAGE = 1 
        {
            PUTBUFFER 
            PUTWRITEIDX 
            GETREADIDX 
        }
        
        GROUP : > CPU2TOCPU1RAM, PAGE = 1
        {
            GETBUFFER :    TYPE = DSECT
            GETWRITEIDX :  TYPE = DSECT
            PUTREADIDX :   TYPE = DSECT
        }  
    
       /* crc/checksum section configured as COPY section to avoid including in executable */
       .TI.memcrc          : type = COPY
        
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

    firmware_issue_txt_file.txt

    firmware_working_txt_file.txt  

    6170.kcontrol_map_file_Not_working.txt

    0804.kcontrol_map_file_working.txt

    Best regards,
    Aditya

  • Ok thanks Aditya, one question, this is using the controlCard correct and not the LaunchPad version of F28379D device?

    Thanks and regards,

    Charles

  • yes using control card, not using launch pad.

    Regards,

    Aditya 

  • Ok thanks, I will need another day to see into this issue, thank you for your patience.

    Regards,

    Charles

  • Hi Aditya,

    From my download of the non-working firmware provided, it gives Incorrect Data Buffer Length error. Is every ALIGN value given in the linker command file ALIGN(8)? Programming of this device should be 128bit aligned. I see in the above linker command file that an ALIGN(4) is present for the BufferDataSection for flash programming.

    How does the working linker command file look from your perspective?

    For the bootloader, are you downloading over SCI_BOOT_ALTERNATE pins for GPIO28/29 communication?

    Is the boot mode set to SCI boot mode, and if so are you testing by setting this mode in CCS memory window (@ address 0xD00, set value as 0x815A, reset CPU1, and run CPU1 before performing firmware update).

    Thanks and regards,

    Charles

  • Hi Charles,

    Yes, we use a custom SCI bootloader that utilizes the SCI_BOOT_ALTERNATE pins for GPIO28/29 communication.

    We identified the issue in the application linker file. To summarize:

    • We encountered program and verify errors at the location labeled "dclfunc."

    • Initially, the DCL functions were combined with the ramfunc section.

    • After making some changes in the application, these errors started appearing, beacuase FLASH sector get full thats why we get Incorrect data buffer length.

    • We then separated the DCL functions into a distinct FLASH sector, which resolved the errors.

    • Additionally, we changed the bufferDataSection alignment to ALIGN(8).

    Please check the application linker .cmd file and let me know if there is any issue in that.

    /*
    //###########################################################################
    // FILE:    flash_programming_cpu1_FLASH.cmd
    // TITLE:   Linker Command File For all F28X7x devices
    //###########################################################################
    // $TI Release: F2837xD Support Library v200 $
    // $Release Date: Tue Jun 21 13:00:02 CDT 2016 $
    // $Copyright: Copyright (C) 2013-2016 Texas Instruments Incorporated -
    //             http://www.ti.com/ ALL RIGHTS RESERVED $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    // The header linker files are found in <base>\F2837xD_headers\cmd
    // For BIOS applications add:      F28X7x_Headers_BIOS.cmd
    // For nonBIOS applications add:   F28X7x_Headers_nonBIOS.cmd
    ========================================================= */
    
    /* Define the memory block start/length for the F28X7x
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
       Notes:
             Memory blocks on F28M3Xx are uniform (ie same
             physical memory) in both PAGE 0 and PAGE 1.
             That is the same memory region should not be
             defined for both PAGE 0 and PAGE 1.
             Doing so will result in corruption of program
             and/or data.
    
             Contiguous SARAM memory blocks or flash sectors can be
             be combined if required to create a larger memory block.
    */
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
              /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
              /* BEGIN is used for the "boot to Flash" bootloader mode   */
    
      BEGIN           	: origin = 0x086000, length = 0x000002
       RAMM0           	: origin = 0x000122, length = 0x0002DE
       RAMD0           	: origin = 0x00B000, length = 0x000800
       RAMLS03          : origin = 0x008000, length = 0x002000
    /*	RAMLS1           : origin = 0x008800, length = 0x000800
        RAMLS2           : origin = 0x009000, length = 0x000800
        RAMLS3           : origin = 0x009800, length = 0x000800 */
       RAMLS4      		: origin = 0x00A000, length = 0x000800
       RAMGS14          : origin = 0x01A000, length = 0x001000
       RAMGS15          : origin = 0x01B000, length = 0x001000
       RESET           	: origin = 0x3FFFC0, length = 0x000002
    
    	/* Flash sectors */
       FLASHA           : origin = 0x080000, length = 0x002000	/* on-chip Flash */
       FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
       FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
       FLASHD           : origin = 0x086002, length = 0x001FFE	/* on-chip Flash */
       FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
       FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
       FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
       FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
       FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
       FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
       FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
       FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
       FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
       FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */
    
    PAGE 1 :   /* Data Memory */
             /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
    
        BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
    	RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
        RAMD1           : origin = 0x00B800, length = 0x000800
    
        RAMLS5      : origin = 0x00A800, length = 0x000800
    
    	RAMGS0          : origin = 0x00C000, length = 0x00B000
    	/*RAMGS1          : origin = 0x00D000, length = 0x001000*/
    	/*RAMGS2          : origin = 0x00E000, length = 0x001000*/
    	/*RAMGS3          : origin = 0x00F000, length = 0x001000
    	RAMGS4          : origin = 0x010000, length = 0x001000
    	RAMGS5          : origin = 0x011000, length = 0x001000
    	RAMGS6          : origin = 0x012000, length = 0x001000
    	RAMGS7          : origin = 0x013000, length = 0x001000
    	RAMGS8          : origin = 0x014000, length = 0x001000
    	RAMGS9          : origin = 0x015000, length = 0x001000
    	RAMGS10         : origin = 0x016000, length = 0x001000*/
    	RAMGS11         : origin = 0x017000, length = 0x001000
    	RAMGS12         : origin = 0x018000, length = 0x001000
    	RAMGS13         : origin = 0x019000, length = 0x001000
    
    
       CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
       CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
    }
    
    
    SECTIONS
    {
    
       /* Allocate program areas: */
       .cinit              : > FLASHD,      PAGE = 0, ALIGN(8)
       .pinit              : > FLASHD,     PAGE = 0, ALIGN(8)
       .text               : >> FLASHE | FLASHH | FLASHI | FLASHJ |FLASHK     PAGE = 0, ALIGN(8)
       codestart           : > BEGIN	PAGE = 0, ALIGN(8)
       
        GROUP
        {
            ramfuncs
            { -l F021_API_F2837xD_FPU32.lib}
         
        } LOAD = FLASHD,
          RUN  = RAMLS03, 
          LOAD_START(_RamfuncsLoadStart),
          LOAD_SIZE(_RamfuncsLoadSize),
          LOAD_END(_RamfuncsLoadEnd),
          RUN_START(_RamfuncsRunStart),
          RUN_SIZE(_RamfuncsRunSize),
          RUN_END(_RamfuncsRunEnd),
          PAGE = 0, ALIGN(8)
    
       dclfuncs : > FLASHG, PAGE = 0, ALIGN(8)
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : >> RAMLS5 | RAMGS0       PAGE = 1
       .esysmem            : > RAMLS5       PAGE = 1
    
       /* Initalized sections go in Flash */
       .econst             : >> FLASHF | FLASHG      PAGE = 0, ALIGN(8)
       .switch             : > FLASHD      PAGE = 0, ALIGN(8)
    
       .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       Filter_RegsFile     : > RAMGS0,	   PAGE = 1
    
       SHARERAMGS0		: > RAMGS0,		PAGE = 1
       SHARERAMGS1		: > RAMGS11,		PAGE = 1
    
       /* Flash Programming Buffer */
       BufferDataSection : > RAMD1, PAGE = 1, ALIGN(8)
       
       /* The following section definitions are required when using the IPC API Drivers */ 
        GROUP : > CPU1TOCPU2RAM, PAGE = 1 
        {
            PUTBUFFER 
            PUTWRITEIDX 
            GETREADIDX 
        }
    
        GROUP : > CPU2TOCPU1RAM, PAGE = 1
        {
            GETBUFFER :    TYPE = DSECT
            GETWRITEIDX :  TYPE = DSECT
            PUTREADIDX :   TYPE = DSECT
        }  
    
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    
    
    
    

    Regards,

    Aditya

  • Hi Charles,

    Please give any suggestion for that.

    Thanks and Regards,

    Aditya

  • Some comparisons between the previous linker and the current working one:

    - Line for .cinit was missing a comma following flash sector assignment

    - dclfuncs and ramfuncs no longer grouped together

    - ramfuncs alone loaded to FLASHD sector (was the sector large enough for both this and dclfuncs?)

    - BufferDataSection using ALIGN(8) directive

    These are the main issues that stand out to me on the difference. Glad you were able to resolve through changing the linker.

    Thanks and regards,

    Charles