Part Number: TMS320F28386D
Other Parts Discussed in Thread: TIDM-02006
Tool/software:
Hello, TI
I am still testing FSI communication.
When I make pwm switching for motor controller. My FSI communication stop.
When I check RJ45(RX_CLK_LVDS_P, RX_CLK_LVDS_N) voltage level.
The level is about 1V attached picture.

Is the voltage level too low, causing the FSI communication to drop when running the motor? Or is the previous voltage level normal?
The FSI CLK voltage to the CPU was measured at 3.3V.
Please some advice..
thank you for reading
Add text (2025.06.25)
Hello, I capture the FSIRxARegs when I run motor and FSI data stop.

what means RX_ECC_LOG is '3' value?
and RX_OPER_CTRL is stoping number is 0x0078, What means this?
thank you for reading