Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Good afternoon,
in our project we are using the TMS320F280049C microcontroller with C2000 Ware 5_04_0_0 and the CLAmath library.
At a certain point of the code (implemented in the .cla file), we are calculating the inverse sine of a float variable by using the CLAasin() function but, during debugging, we noticed that if the float number get close to values equal to 1, the function does not return values equal to PI/2 (1.570796...). The values we get are lower.
Just for verification, we tried also to provide a constant float equal to 1 as a argument of the CLAasin() function, but still we get lower values than PI/2 (1.570796...). Same results if we use the CLAasin_inline() function.
Can you please help us on this topic?
Thank you in advance,
Marco R. De Cesero