Part Number: LAUNCHXL-F28P55X
Tool/software:
I am using LAUNCHXL-F28P55X with BoostXL-3PhGaN.
1. On the first debug the error appeared:
IcePick_C_0: Error: (Error -591 @ 0x0) The firmware updater encountered an error and could not finish. The updater failed to connect to the XDS110 in programming mode. Unplug and re-plug the XDS110, and try again. If the problem remains, try updating the firmware using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of the installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 20.0.0.3178
2. I used xdsdfu from the command prompt to update it to firmware firmware_3.0.0.32 (following the pdf guide of xds110 online)

3. I restarted the computer is debugged again, now this error appears:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 20.0.0.3178)
I opened the ccxml file from here:

4. and I ran “test connection,” this message appears:
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\DEBART~1\AppData\Local\TEXASI~1\
CCS\ccs1281\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Sep 26 2024'.
The library build time was '10:09:41'.
The library package version is '20.0.0.3178'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End: Texas Instruments XDS110 USB Debug Probe_0]
What to do?