Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE, MSPM0G3505
Tool/software:
When going through the EQEP lab in the C28x academy tutorials none of the position variables are updating. I've gone through and checked signals (I don't have an oscilloscope right now so I just used the onboard ADC). I have the correct pins for my A,B, and I signals. The register read is just not updating with any values. Checking the solution in the training for f28004x there are settings that are different from the tutorial in the sysconfig. Neither the tutorial or the given solution update the values. The go into the ISR and pass the base check and then go to reading the register but the value is not counting which seems like it's not enabled properly seeing as the PWM signals for testing appear correct. Not sure where to go from here as I need to use the EQEP for my controller so help would be appreciated.