This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: CAN configure question

Part Number: TMS320F28069

Tool/software:

Hi expert,

Currently customer (CosMX) set up the CAN periodic 100ms send data. The ABO bus self-recovery feature is enabled because the CAN bus can experience interference from hanging-dead conditions. Can customer continue to re-transmit without successful data after CAN bus recovery? Or do we need to wait for the next cycle 100ms to retransmit? We checked the 28069 manual and couldn't find the corresponding function which doesn't allow resending. I saw the 28377 which doesn't allow resending, but the 28069 couldn't find it, so please help to confirm. Thanks.

  • 28069 manual:

  • 28377D manual:

Best Regards,

Ryker