This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: dacn boot

Part Number: TMS320F2800137

Tool/software:

Hello, this is the official code from TI, but it is a dacn boot for f28003x. I tried porting it to f2800137 and found that communication was normal, And C0 7a was added to the boot program, combined with serial port burning boot, and it was found that the memory was edited to 128 bits every time. It was confirmed that the burning process had entered because I wrote a fixed CAN to send a message, as shown in line 189. Finally, I found that the program was completely erased, but there was no writing. Is there anything else I didn't pay attention to

//###########################################################################
//
// FILE:    flash_kernel_ex5_boot.c
//
// TITLE:   Boot loader shared functions
//
//###########################################################################
// $TI Release: F280015x Support Library v5.03.00.00 $
// 
// $Copyright:
// Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "ex_5_cpu1bootrom.h"
#include "cpu1brom_utils.h"
#include "FlashTech_F280013x_C28x.h"
#include "flash_programming_f280013x.h"
#include "driverlib.h"

#define BUFFER_SIZE               0x400
#define DCAN_MAX_BUFFER_SIZE        8U
#define LOWER_FIRST_BLOCK_SIZE      6U
#define UPPER_FIRST_BLOCK_SIZE      7U
#define DCAN_MAX_PAYLOAD_BYTES      8U

#define DCSM_OTP_Z1_LNKPTR_START 0x78000
#define DCSM_OTP_Z1_LNKPTR_END   0x78020

#define DCSM_OTP_Z2_LNKPTR_START 0x78200
#define DCSM_OTP_Z2_LNKPTR_END   0x78220

typedef enum
{
    DCAN_DATA_SIZE_16BITS = 2U,
    DCAN_DATA_SIZE_32BITS = 4U
}DCAN_dataTypeSize;


/**
 * \brief  Structure for DCAN Rx Buffer element.
 */
typedef struct
{
    uint16_t  data[DCAN_MAX_PAYLOAD_BYTES];
    /**< Data bytes.
     *   Only first dlc number of bytes are valid.
     */
}DCAN_RxBufElement;

//
// GetWordData is a pointer to the function that interfaces to the peripheral.
// Each loader assigns this pointer to it's particular GetWordData function.
//
extern uint16fptr GetWordData;
extern uint32_t findSector(uint32_t address);
extern uint16_t findSize(uint32_t address);
//
// miniBuffer: Useful for 4-word access to flash
//
uint16_t miniBuffer[8];

//
// Function prototypes
//
uint32_t GetLongData();
void CopyData(void);
//void CopyApplication(DCAN_RxBufElement rxMsg, uint32_t WE_Protection_Mask_A,
//                        uint32_t WE_Protection_Mask_B, uint32_t WE_Protection_Mask_UO);
void DCSM_OTP_Write(uint32_t destAddr, uint16_t* miniBuffer, uint32_t WE_Protection_Mask_UO);
void ReadReservedFn(void);
extern void sharedErase(uint32_t sectors);
uint16_t DCAN_GetWordData(void);
extern uint32_t DCAN_getDataFromBuffer(DCAN_dataTypeSize dataTypeSize);
extern uint16_t msgBufferIndex;
void Example_Error();
void DCAN_SendWordData_test(uint16_t data);
//
// CopyApplication - This routine copies multiple blocks of data from the host
//                   to the specified Flash locations. It is assumed that the
//                   application is linked to Flash correctly and that the image is
//                   512 bit aligned. Errors from the Flash API are not currently
//                   being relayed to the host.
//
//                   Multiple blocks of data are copied until a block
//                   size of 00 00 is encountered.
//

void CopyApplication(DCAN_RxBufElement rxMsg)
{
    struct HEADER {
      uint16_t BlockSize;
      uint32_t DestAddr;
    } BlockHeader;

    uint16_t i = 0;
    uint16_t j = 0;
    uint16_t k = 0;
    uint16_t fail = 0;
    uint32_t sectorAddress;
    uint16_t sectorSize;
    uint16_t wordsWritten = 0;

    //
    // wordData: Stores a word of data
    //
    uint16_t wordData;

    //
    // miniBuffer: Useful for 4-word access to flash
    //
    uint16_t miniBuffer[8];

    //
    // Buffer: Used to program data to flash
    //
    uint16_t Buffer[BUFFER_SIZE];

    //
    // Error return variable
    //
    Fapi_StatusType oReturnCheck;

    //
    // FAPI initialization
    //
#if 0
    Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, 120);
    oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);

    if(oReturnCheck != Fapi_Status_Success)
    {
        return;
    }
#endif
    //
    // Get the size in words of the first block
    //
    BlockHeader.BlockSize = BUILD_WORD(rxMsg.data[LOWER_FIRST_BLOCK_SIZE],
                                       rxMsg.data[UPPER_FIRST_BLOCK_SIZE]);

    //
    // Set the message buffer index for reading next stream data
    //
    msgBufferIndex = UPPER_FIRST_BLOCK_SIZE + 1U;

    //
    // While the block size is > 0 flash the data
    // to the DestAddr.  There is no error checking
    // as it is assumed the DestAddr is a valid
    // memory location
    //
    while(BlockHeader.BlockSize != (uint16_t)0x0000)
    {
            Fapi_StatusType oReturnCheck;
            Fapi_FlashStatusWordType oFlashStatusWord;
            Fapi_FlashStatusType oFlashStatus;
            DCAN_SendWordData_test(0x1245);

            BlockHeader.DestAddr = DCAN_getDataFromBuffer(DCAN_DATA_SIZE_32BITS);

            //
            // Iterate through the block of data in order to program the data
            // in flash
            //
            for (i = 0; i < BlockHeader.BlockSize; i += 0)
            {
                //
                // If the size of the block of data is less than the size of the buffer,
                // then fill the buffer with the block of data and pad the remaining
                // elements
                //
                if (BlockHeader.BlockSize < BUFFER_SIZE)
                {
                    //
                    // Receive the block of data one word at a time and place it in
                    // the buffer
                    //
                    for (j = 0; j < BlockHeader.BlockSize; j++)
                    {
                        //
                        // Receive one word of data
                        //
                        wordData = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));

                        //
                        // Put the word of data in the buffer
                        //
                        Buffer[j] = wordData;

                        //
                        // Increment i to keep track of how many words have been received
                        //
                        i++;
                    }

                    //
                    // Pad the remaining elements of the buffer
                    //
                    for (j = BlockHeader.BlockSize; j < BUFFER_SIZE; j++)
                    {
                        //
                        // Put 0xFFFF into the current element of the buffer. OxFFFF is equal to erased
                        // data and has no effect
                        //
                        Buffer[j] = 0xFFFF;
                    }
                }

                //
                // Block is to big to fit into our buffer so we must program it in
                // chunks
                //
                else
                {
                    //
                    // Less than one BUFFER_SIZE left
                    //
                    if ((BlockHeader.BlockSize - i) < BUFFER_SIZE)
                    {
                        //
                        // Fill Buffer with rest of data
                        //
                        for (j = 0; j < BlockHeader.BlockSize - i; j++)
                        {
                           //
                           // Receive one word of data
                           //
                           wordData = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));

                           //
                           // Put the word of data into the current element of Buffer
                           //
                           Buffer[j] = wordData;
                        }

                        //
                        // Increment i outside here so it doesn't affect loop above
                        //
                        i += j;

                        //
                        // Fill the rest with 0xFFFF
                        //
                        for (; j < BUFFER_SIZE; j++)
                        {
                           Buffer[j] = 0xFFFF;
                        }
                    }
                    else
                    {
                        //
                        // Fill up like normal, up to BUFFER_SIZE
                        //
                        for (j = 0; j < BUFFER_SIZE; j++)
                        {
                           wordData = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));
                           Buffer[j] = wordData;
                           i++;
                        }
                    }
                }

                //
                // Fill miniBuffer with the data in Buffer in order to program the data
                // to flash; miniBuffer takes data from Buffer, 88 words at a time.
                //
                for (k = 0; k < (BUFFER_SIZE / 8); k++)
                {
                    miniBuffer[0] = Buffer[k * 8 + 0];
                    miniBuffer[1] = Buffer[k * 8 + 1];
                    miniBuffer[2] = Buffer[k * 8 + 2];
                    miniBuffer[3] = Buffer[k * 8 + 3];
                    miniBuffer[4] = Buffer[k * 8 + 4];
                    miniBuffer[5] = Buffer[k * 8 + 5];
                    miniBuffer[6] = Buffer[k * 8 + 6];
                    miniBuffer[7] = Buffer[k * 8 + 7];

                    //
                    // check that all the words have not already been written
                    //
                    if (wordsWritten < BlockHeader.BlockSize)
                    {
                        if(fail == 0)
                        {
                            //
                            // clean out flash banks if needed
                            //
                            sectorAddress = findSector(BlockHeader.DestAddr);
                            if (sectorAddress != 0xdeadbeef)
                            {
                                //
                                // FindSize just returns 0x4000.
                                //
                                sectorSize = findSize(sectorAddress);
                                Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROTA, 0);
                                Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROTB, 0);

                                oReturnCheck = Fapi_issueAsyncCommandWithAddress(
                                        Fapi_EraseSector, (uint32_t *) sectorAddress);

                                while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}

                                oFlashStatus = Fapi_getFsmStatus();

                                oReturnCheck = Fapi_doBlankCheck(
                                        (uint32_t *) sectorAddress, sectorSize,
                                        &oFlashStatusWord);
                                if (oReturnCheck != Fapi_Status_Success || oFlashStatus != 0)
                                {
                                    fail++;
                                }
                            }
                        }
                        if(fail == 0)
                        {
                            //
                            //program 8 words at once, 128-bits
                            //
                            oReturnCheck = Fapi_issueProgrammingCommand(
                                    (uint32_t *) BlockHeader.DestAddr, miniBuffer,
                                    sizeof(miniBuffer), 0, 0, Fapi_AutoEccGeneration);

                            while (Fapi_checkFsmForReady() == Fapi_Status_FsmBusy);

                            oFlashStatus = Fapi_getFsmStatus();

                            if (oReturnCheck != Fapi_Status_Success || oFlashStatus != 0)
                            {
                                fail++;
                            }
                        }
                        for (j = 0; j < 8; j += 2)
                        {
                            uint32_t toVerify = miniBuffer[j + 1];
                            toVerify = toVerify << 16;
                            toVerify |= miniBuffer[j];
                            if(fail == 0)
                            {
                                oReturnCheck = Fapi_doVerify(
                                        (uint32_t *) (BlockHeader.DestAddr + j), 1,
                                        (uint32_t *) (&toVerify), &oFlashStatusWord);
                                if (oReturnCheck != Fapi_Status_Success)
                                {
                                    fail++;
                                }
                            }
                        } //for j; for Fapi_doVerify
                    } //check if all the words are not already written
                    BlockHeader.DestAddr += 0x8;
                    wordsWritten += 0x8;
                } //for(int k); loads miniBuffer with Buffer elements
        }
        //
        // Get the size of the next block
        //
        BlockHeader.BlockSize = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));
        wordsWritten = 0;
    }
    return;
}















#if 0
void CopyApplication(DCAN_RxBufElement rxMsg, uint32_t WE_Protection_Mask_A, 
                        uint32_t WE_Protection_Mask_B, uint32_t WE_Protection_Mask_UO)
{
    struct HEADER {
      uint16_t BlockSize;
      uint32_t DestAddr;
    } BlockHeader;

    uint16_t i = 0;
    uint16_t j = 0;
    uint16_t k = 0;
    uint16_t fail = 0;
    uint16_t wordsWritten = 0;

    //Fapi_StatusType oReturnCheck;
    Fapi_FlashStatusWordType oFlashStatusWord;
    Fapi_FlashStatusType oFlashStatus;

    //
    // wordData: Stores a word of data
    //
    uint16_t wordData;

    //
    // Buffer: Used to program data to flash
    //
    uint16_t Buffer[BUFFER_SIZE];

    //
    // Error return variable
    //
    Fapi_StatusType oReturnCheck;


    //
    // Get the size in words of the first block
    //
    BlockHeader.BlockSize = BUILD_WORD(rxMsg.data[LOWER_FIRST_BLOCK_SIZE],
                                       rxMsg.data[UPPER_FIRST_BLOCK_SIZE]);

    //
    // Set the message buffer index for reading next stream data
    //
    msgBufferIndex = UPPER_FIRST_BLOCK_SIZE + 1U;

    //
    // While the block size is > 0 flash the data
    // to the DestAddr.  There is no error checking
    // as it is assumed the DestAddr is a valid
    // memory location
    //
    while(BlockHeader.BlockSize != (uint16_t)0x0000)
    {
            // Initialize flag to keep track if writing to OTP or not
            uint16_t otpFlag = 0;
            DCAN_SendWordData_test(0x1245);
            // Get destination address of block
            BlockHeader.DestAddr = DCAN_getDataFromBuffer(DCAN_DATA_SIZE_32BITS);

            // Check destination address to see if we are writing to OTP
            if ((BlockHeader.DestAddr >= OTP_MAP_BEGIN) && (BlockHeader.DestAddr <= OTP_MAP_END)) 
            {
                otpFlag = 1;
            }

            //
            // Iterate through the block of data in order to program the data
            // in flash
            //
            for (i = 0; i < BlockHeader.BlockSize; i += 0)
            {
                //
                // If the size of the block of data is less than the size of the buffer,
                // then fill the buffer with the block of data and pad the remaining
                // elements
                //
                if (BlockHeader.BlockSize < BUFFER_SIZE)
                {
                    //
                    // Receive the block of data one word at a time and place it in
                    // the buffer
                    //
                    for (j = 0; j < BlockHeader.BlockSize; j++)
                    {
                        //
                        // Receive one word of data
                        //
                        wordData = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));

                        //
                        // Put the word of data in the buffer
                        //
                        Buffer[j] = wordData;

                        //
                        // Increment i to keep track of how many words have been received
                        //
                        i++;
                    }

                    //
                    // Pad the remaining elements of the buffer
                    //
                    for (j = BlockHeader.BlockSize; j < BUFFER_SIZE; j++)
                    {
                        //
                        // Put 0xFFFF into the current element of the buffer. OxFFFF is equal to erased
                        // data and has no effect
                        //
                        Buffer[j] = 0xFFFF;
                    }
                }

                //
                // Block is too big to fit into our buffer so we must program it in
                // chunks
                //
                else
                {
                    //
                    // Less than one BUFFER_SIZE left
                    //
                    if ((BlockHeader.BlockSize - i) < BUFFER_SIZE)
                    {
                        //
                        // Fill Buffer with rest of data
                        //
                        for (j = 0; j < BlockHeader.BlockSize - i; j++)
                        {
                           //
                           // Receive one word of data
                           //
                           wordData = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));

                           //
                           // Put the word of data into the current element of Buffer
                           //
                           Buffer[j] = wordData;
                        }

                        //
                        // Increment i outside here so it doesn't affect loop above
                        //
                        i += j;

                        //
                        // Fill the rest with 0xFFFF
                        //
                        for (; j < BUFFER_SIZE; j++)
                        {
                           Buffer[j] = 0xFFFF;
                        }
                    }
                    else
                    {
                        //
                        // Fill up like normal, up to BUFFER_SIZE
                        //
                        for (j = 0; j < BUFFER_SIZE; j++)
                        {
                           wordData = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));
                           Buffer[j] = wordData;
                           i++;
                        }
                    }
                }

                // If writing to 512 bits of DCSM OTP containing link pointers, write 64-bits at a time
                if ((BlockHeader.DestAddr >= DCSM_OTP_Z1_LNKPTR_START) && (BlockHeader.DestAddr < DCSM_OTP_Z1_LNKPTR_END) || 
                (BlockHeader.DestAddr >= DCSM_OTP_Z2_LNKPTR_START) && (BlockHeader.DestAddr < DCSM_OTP_Z2_LNKPTR_END))
                {

                    //
                    // Fill miniBuffer with the data in Buffer in order to program the data
                    // to flash; miniBuffer takes data from Buffer, 88 words at a time.
                    //
//                    for (k = 0; k < (BUFFER_SIZE / 4); k++)
//                    {
//                        uint16_t bufferOffset = k * 4;
//
//                        miniBuffer[0] = Buffer[bufferOffset + 0];
//                        miniBuffer[1] = Buffer[bufferOffset + 1];
//                        miniBuffer[2] = Buffer[bufferOffset + 2];
//                        miniBuffer[3] = Buffer[bufferOffset + 3];

                    for (k = 0; k < (BUFFER_SIZE / 8); k++)
                       {
                           miniBuffer[0] = Buffer[k * 8 + 0];
                           miniBuffer[1] = Buffer[k * 8 + 1];
                           miniBuffer[2] = Buffer[k * 8 + 2];
                           miniBuffer[3] = Buffer[k * 8 + 3];
                           miniBuffer[4] = Buffer[k * 8 + 4];
                           miniBuffer[5] = Buffer[k * 8 + 5];
                           miniBuffer[6] = Buffer[k * 8 + 6];
                           miniBuffer[7] = Buffer[k * 8 + 7];



                        //
                        // check that all the words have not already been written
                        //
                        if (wordsWritten < BlockHeader.BlockSize)
                        {

                            DCSM_OTP_Write(BlockHeader.DestAddr, miniBuffer, WE_Protection_Mask_UO);                         

                        } //check if all the words are not already written
                        BlockHeader.DestAddr += 0x8;
                        wordsWritten += 0x8;
                    } 
                } 
                else 
                {
                    //
                    // check that all the words have not already been written
                    //
                    if (wordsWritten < BlockHeader.BlockSize)
                    {
                        if(fail == 0)
                        {
                            //
                            //program 32 words at once, 512-bits
                            //
                            //

                            // Disable erase/program protection
                            if (otpFlag) 
                            {
                                Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROT_UO, WE_Protection_Mask_UO);
                            }
                            else 
                            {
                                //

                                // Bits 0-11 of CMDWEPROTB is applicable for sectors 32-127, each bit represents
                                // a group of 8 sectors, e.g bit 0 represents sectors 32-39, bit 1 represents
                                // sectors 40-47, etc
                                //
                                Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROTA, WE_Protection_Mask_A);
                                Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROTB, WE_Protection_Mask_B);
                            }

                            oReturnCheck = Fapi_issueAutoEcc512ProgrammingCommand((uint32_t *) BlockHeader.DestAddr,
                                                                                  Buffer, sizeof(Buffer));

                            while (Fapi_checkFsmForReady() == Fapi_Status_FsmBusy);

                            oFlashStatus = Fapi_getFsmStatus();

                            if (oReturnCheck != Fapi_Status_Success || oFlashStatus != 3)
                            {
                                fail++;
                            }
                        }

                        // Only verify if we are not writing to DCSM
                        if (!(otpFlag))
                        {
                            
                            oReturnCheck = Fapi_doVerify((uint32_t *) (BlockHeader.DestAddr), 16, (uint32_t*) Buffer, &oFlashStatusWord);
                            if (oReturnCheck != Fapi_Status_Success) 
                            {
                                fail++;
                            }

                        }


                    } 
                    BlockHeader.DestAddr += 0x08;
                    wordsWritten += 0x08;
                }

        }
        //
        // Get the size of the next block
        //
        BlockHeader.BlockSize = (uint16_t)(DCAN_getDataFromBuffer(DCAN_DATA_SIZE_16BITS));
        wordsWritten = 0;
    }
    return;
}
#endif
// DCSM_OTP_Write is used to write 64-bits to DCSM OTP 
// This is needed because we cannot write 128 or 512 bits to the link pointers
void DCSM_OTP_Write(uint32_t destAddr, uint16_t* miniBuffer, uint32_t WE_Protection_Mask_UO)
{
    Fapi_FlashStatusType oFlashStatus;

    //
    // Error return variable
    //
    Fapi_StatusType oReturnCheck;

    //
    //program 4 words at once, 64-bits
    //
    //

    //
    // Disable erase/program protection
    Fapi_setupBankSectorEnable(FLASH_WRAPPER_PROGRAM_BASE+FLASH_O_CMDWEPROT_UO, WE_Protection_Mask_UO);

    oReturnCheck = Fapi_issueProgrammingCommand((uint32_t *) destAddr, miniBuffer,
                                                4, 0, 0, Fapi_AutoEccGeneration);

    while (Fapi_checkFsmForReady() == Fapi_Status_FsmBusy);

    oFlashStatus = Fapi_getFsmStatus();

    if (oReturnCheck != Fapi_Status_Success || oFlashStatus != 3)
    {
        Example_Error();
    }

}

//
// getLongData -    Fetches a 32-bit value from the peripheral
//                  input stream.
//

uint32_t GetLongData(void)
{
    uint32_t longData;

    //
    // Fetch the upper 1/2 of the 32-bit value
    //
    longData = ( (uint32_t)(*GetWordData)() << 16);

    //
    // Fetch the lower 1/2 of the 32-bit value
    //
    longData |= (uint32_t)(*GetWordData)();

    return longData;
}

//
// Read_ReservedFn -    Reads 8 reserved words in the header.
//                      None of these reserved words are used by the
//                      this boot loader at this time, they may be used in
//                      future devices for enhancments.  Loaders that use
//                      these words use their own read function.
//

void ReadReservedFn(void)
{
    uint16_t i;

    //
    // Read and discard the 8 reserved words.
    //
    for(i = 1; i <= 8; i++)
    {
       GetWordData();
    }
    return;
}

void Example_Error()
{
    asm(" ESTOP0");
}


#define CAN_MSG_OBJ_2          0x2U
void DCAN_SendWordData_test(uint16_t data)
{
    HWREG_BP(CANA_BASE + CAN_O_IF2DATA) = data;
    HWREG_BP(CANA_BASE + CAN_O_IF2CMD) = (uint32_t)(CAN_IF2CMD_DIR |
                                                    CAN_IF2CMD_TXRQST |
                                                    CAN_IF2CMD_DATA_A |
                                                    CAN_IF2CMD_DATA_B |
                                                    CAN_MSG_OBJ_2);

    NOP_CYCLES(255);

    while((HWREGH(CANA_BASE + CAN_O_IF2CMD) & CAN_IF2CMD_BUSY) == CAN_IF2CMD_BUSY)
    {
    }

    while((HWREGH(CANA_BASE + CAN_O_TXRQ_21) & CAN_MSG_OBJ_2) == CAN_MSG_OBJ_2)
    {
    }
}

  • Hi Zhou, 

    I recommend starting with the F280015x DCAN flash kernel example when porting to F280013x. The devices are very similar so it will be easier than porting from F28003x. Can you send a copy of the .txt file you are attempting to program to flash?

    Kind regards,

    Skyler

  • According to manuals F28003x and 137, it was found that the memory is edited to 128 bits each time, while F280015x is 512 bits. Therefore, the program burning borrowed F28003x and used a baud rate of 100k instead of 1000k, just like 03x. The third and fourth bytes of the boot program were set to 0 by default, and attempts were made to change it to 1000k. The boot program also changed, but did not return the set message. 100k returned a fixed message


    The txt file attempting to program is sent to flash memory. The bootloader successfully imported and sent a fixed message, but the application cannot write it properly. There are two issues with sending it first
    1. It seems that the sector has not been found and has not entered the statement
    2. BlockHeader.BlockSize defines the byte count for reading CAN messages as 6 and 7, but I have noticed that sometimes bytes such as 1, 2, or 2, 3 are also read, resulting in misalignment
    3 Does 137 default to 100k? I found that a routine also uses 100k,

    C:\Users\Lenovo\workspace_v12\tida_010273_GaNInv_f280013x\src_device\boot_rom\include\bootloader_can_timing.h

  • Hi Zhou,

    It seems that you've opened another thread for this topic, so I am closing this thread for now.

    Kind regards,

    Skyler