This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H850TU: Assembler documentation

Part Number: F29H850TU

Tool/software:

Since we implement the interrupt-entry and exception-context code in assembly to maintain fine-grained control, could you please confirm whether there is detailed documentation for the assembler itself (in addition to the instruction set that we already have)? This would include information on directives and syntax. If so, can it be provided to support our development?

We need clarification on defining macros with parameters. With other LLVM TI compilers we've successfully used:

.macro MacroName, Params
/* Macro definition */
.endm

But on the C29x we could not define parameters along with macro. Because we rely heavily on parameterized macros in our exception and interrupt-entry code, understanding the correct syntax for the C29x assembler is essential for us.

  • Hi George,

    The question about defining a macro with parameters actually comes from me. I see in the Clang document (sourceware.org/.../Macro.html that we can use .macro MacroName, Params to define parameters. However, the assembler does not recognize the parameters, resulting in an undefined symbol error during linking. To reproduce this issue, I modified the source file kernel/freertos/Source/portable/CCS/C2000_C29x/portasm.asm in the SDK.

    I defined a loadNum macro with the address parameter.

    .macro loadNum address
        LD.32 A14, @address
    .endm
    Then I call it in vPortYield:
    loadNum pxCurrentTCB
    Then during linking I get the error:
     undefined first referenced
      symbol       in file
     --------- ----------------
     address   C:\Users\xchen\AppData\Local\Temp\portasm-f02d2f.o
    
    error: unresolved symbols remain
    error: errors encountered during linking; "SOM/FLASH/control+rtos_demo.out" not
       built
    c29clang: error: c29lnk command failed with exit code 1 (use -v to see invocation)

    I use the makefile-based build to compile the example. gmake -s control+rtos_demo PROFILE=debug_O0 CONFIG=FLASH"

    Used compiler: "TI C29 Clang Compiler 1.0.0.LTS."

    I have also attached the modified portasm.asm file:

        .extern pxCurrentTCB
        .extern bYield
        .extern bPreemptive
        .extern ulCriticalNesting
        .extern xTaskIncrementTick
        .extern vTaskSwitchContext
        .extern ulTaskHasFPUContext
    
        .global portTICK_ISR
        .global portRESTORE_FIRST_CONTEXT
        .global vPortYield
        .global profile1_start, profile1_end, profile2_start, profile2_end
    
        .macro loadNum address
            LD.32 A14, @address
        .endm
    
        .macro portSAVE_CONTEXT
            ST.32 *(A15++#8), A14
            || MV A14, RPC
            ST.32 *(A15-#4), A14
            ST.32 *(A15++#8), DSTS
            ST.32 *(A15-#4), ESTS
            ST.64 *(A15++#8), XA0
            ST.64 *(A15++#8), XA2
            ST.64 *(A15++#8), XA4
            ST.64 *(A15++#8), XA6
            ST.64 *(A15++#8), XA8
            ST.64 *(A15++#8), XA10
            ST.64 *(A15++#8), XA12
            ST.64 *(A15++#8), XD0
            ST.64 *(A15++#8), XD2
            ST.64 *(A15++#8), XD4
            ST.64 *(A15++#8), XD6
            
            ;Check if task has FPU context
            || LD.32	 D0, @ulTaskHasFPUContext
    
            ST.64 *(A15++#8), XD8
            || BCMPZD  .+0x54, D.EQ, D0
            ST.64 *(A15++#8), XD10
            ST.64 *(A15++#8), XD12
            ST.64 *(A15++#8), XD14
    
            ST.64 *(A15++#8), XM0
            ST.64 *(A15++#8), XM2
            ST.64 *(A15++#8), XM4
            ST.64 *(A15++#8), XM6
            ST.64 *(A15++#8), XM8
            ST.64 *(A15++#8), XM10
            ST.64 *(A15++#8), XM12
            ST.64 *(A15++#8), XM14
            ST.64 *(A15++#8), XM16
            ST.64 *(A15++#8), XM18
            ST.64 *(A15++#8), XM20
            ST.64 *(A15++#8), XM22
            ST.64 *(A15++#8), XM24
            ST.64 *(A15++#8), XM26
            ST.64 *(A15++#8), XM28
            ST.64 *(A15++#8), XM30
    
            ; Store FPU context indicator
            ST.32 *(A15++#8), D0 
            ; Store the new top of stack for the task.
            || LD.32	A14, @pxCurrentTCB
            ST.32	*A14, A15
        .endm
    
        .macro portRESTORE_CONTEXT
            LD.32 A0, @pxCurrentTCB
            LD.32 A15, *A0
    
            ;Check if task has FPU context
            LD.32	 D0, *(A15-=#8)
            ST.32 @ulTaskHasFPUContext, D0
            || BCMPZ  .+0x4a, D.EQ, D0
    
            LD.64 XM30, *(A15-=#8)
            LD.64 XM28, *(A15-=#8)
            LD.64 XM26, *(A15-=#8)
            LD.64 XM24, *(A15-=#8)
            LD.64 XM22, *(A15-=#8)
            LD.64 XM20, *(A15-=#8)
            LD.64 XM18, *(A15-=#8)
            LD.64 XM16, *(A15-=#8)
            LD.64 XM14, *(A15-=#8)
            LD.64 XM12, *(A15-=#8)
            LD.64 XM10, *(A15-=#8)
            LD.64 XM8,  *(A15-=#8)
            LD.64 XM6,  *(A15-=#8)
            LD.64 XM4,  *(A15-=#8)
            LD.64 XM2,  *(A15-=#8)
            LD.64 XM0,  *(A15-=#8)
            
            LD.64 XD14, *(A15-=#8)
            LD.64 XD12, *(A15-=#8)
            LD.64 XD10, *(A15-=#8)
            LD.64 XD8,  *(A15-=#8)
            LD.64 XD6,  *(A15-=#8)
            LD.64 XD4,  *(A15-=#8)
            LD.64 XD2,  *(A15-=#8)
            LD.64 XD0,  *(A15-=#8)
            LD.64 XA12, *(A15-=#8)
            LD.64 XA10, *(A15-=#8)
            LD.64 XA8,  *(A15-=#8)
            LD.64 XA6,  *(A15-=#8)
            LD.64 XA4,  *(A15-=#8)
            LD.64 XA2,  *(A15-=#8)
            LD.64 XA0,  *(A15-=#8)
            LD.32 DSTS, *(A15-=#8)
            LD.32 ESTS, *(A15+#4)
            LD.32 A14,  *(A15-=#8)
            LD.32 RPC,  *(A15+#4)
    
        .endm
    
    portTICK_ISR:
    profile1_start:
    	; Save the context of the current task.
        portSAVE_CONTEXT
    profile1_end:
    
        ;ENINT
    
        ; Increment tick counter
        CALL     xTaskIncrementTick
        BCMPZ    skipTaskSwitchContext, D.EQ, D0
        CALL     @vTaskSwitchContext
    
    skipTaskSwitchContext:
    profile2_start:
        ; Restore the context of the task selected to execute.
        portRESTORE_CONTEXT
    profile2_end:
    
        RETI.INT
    
    
    vPortYield:
    	; Save the context of the current task.
        portSAVE_CONTEXT
        loadNum pxCurrentTCB
    
        ;ENINT
    
        ; Select the next task to execute.
        CALL      @vTaskSwitchContext
    
        ; Restore the context of the task selected to execute.
        portRESTORE_CONTEXT
        RETI.INT
    
    
    portRESTORE_FIRST_CONTEXT:
        portRESTORE_CONTEXT
        RET

    Many thanks in advance.

  • I just realized I forgot the \ before address, so the correct macro should be

        .macro loadNum address
            LD.32 A14, @\address
        .endm

    Therefore the problem is resolved. Thank you very much.