Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMDSCNCD28379D, C2000WARE
Tool/software:
Dear TI Support,
One of my customers would like to use a USB flash to load the firmware during the production process.
I am currently working on this at the firmware level, but I noticed that we need to connect via the XDS debugger to change a register value before we can flash using USB.
Specifically, we have to write 0x0C5A to the boot mode select address (0xD00) using the debugger.
The issue is that the person responsible for flashing the code in production has never used Code Composer Studio (CCS), and there won’t be a JTAG debugger available on the production line.
Could you please clarify this point: Is it necessary to write 0x0C5A to RAM every time before flashing via USB? Or is there a way to automate or embed this step so that USB flashing can be performed without a debugger?
Ultimately, my goal is to be able to load the initial firmware using only a USB on CPU1 and CPU2 flash drive during production. Is this feasible?
Thank you for your support.
Best regards,
S. Tarik