Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG, CONTROLSUITE, SFRA
Tool/software:
Hi TI team,
I'm trying to run tidm_02000 solution found in → C:\ti\c2000\C2000Ware_DigitalPower_SDK_5_05_01_00\solutions\tidm_02000\f28004x\ccs
I'm using the project → import CCS project method to open the folder CCS project file name → PCMC_PSFB_F28004x but I'm facing a problem running Compensation Designer in main.syscfg file
1- when I try select INCR_BUILD as closed voltage loop and try to run Compensation Designer some times it do run and some times it won't also if delete the project and import it again it doesn't run again
2- If i rebuild the project while INCR_BUILD selected as closed voltage loop it gives me the error shown in the picture below, but if I rebuild the project when open voltage loop selected the error in the pic below disappears
My system :
C2000Ware_DigitalPower_SDK_5_05_01_00
C2000Ware_v5.04.00.00 installed with Digital power sdk package
CCS12.8.1.00005_win64
sysconfig_1.24.1
controlSUITE
win 11