This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Liu,
http://www.ti.com/lit/an/spraal3/spraal3.pdf
Are you using Serial Solution provided in section 3 of Flash Programming Solutions for the TMS320F28xxx DSCs?
Also, I would first confirm whether SCI module works by running SCI examples provided in (C280x, C2801x C/C++ Header Files and Peripheral Examples )
Regards,
Manoj
Manoj,
I had tried the method of SDFlash programming a weeks ago,before I used the C2Prog.The same as C2Prog,I failed, because the communication also can not be established when I click the program button in SDFlash.The Dsp can communicate with the PC correctly when it runs the normal program over the RS232 cable.I use C2Prog
or SDFlash all as the help documents bidding with these softwate step by step. I do not know what I do not do right.
Liu
Liu,
I have never used C2Prog to program flash. However, I have programmed flash using SDflash. I used the following document (http://emulators.spectrumdigital.com/utilities/sdflash/c2000/SDFlash_Serial_RefGuide_v3_3.pdf) to program the flash. Please use this as reference.
Not sure how I can be of much help without looking at your hardware setup.
Regards,
Manoj