Part Number: F29H85X-SOM-EVM
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
SysConfig limits the speed of the UART to 921600 baud. The datasheet mentions in the UART section 6.19.9, "Programmable baud-rate generator allowing speeds of up to 12.5Mbps for regular speed (divide by 16) and
25Mbps for high speed (divide by 8)". Is the speed mentioned in the datasheet achievable? If so, does it need to be manually configured outside SysConfig?
Thank you!