Part Number: F29H85X-SOM-EVM
Tool/software:
Hi Experts,
I'm trying to create a empty section with a set address that I could update the section with a binary image from another build project. So far, this is what I have specified in the linker script
SECTIONS
{
...
cpu1_app : {} fill(0) > 0x10018000, type=COPY, START(app1EntryAddr)
}
And it does generate an empty section with the set address:

In my post build step within CCS, I used c29objcopy to update this section with a custom application image via:
${CG_TOOL_OBJCOPY} --update-section cpu1_app=../../cpu1_firmware.bin ${ProjName}.out ${ProjName}_firmware.out
And the result for the most part is what I expected (replaces the cpu1_app section with a real section that has offsets and addresses)

However, every once a while a failure occurs when I wanted to convert the .out image into binary:

It seems to be complaining about the elf format. And this failure only comes up randomly.
(Note I didn't populate map any code/variables to this cpu1_app. I'm relying on fill(0) to bypass the size checks in this section when updated by c29objcopy )
Is there any suggestions on how can I solve this issue? Or please recommend me the best way to generate and update empty sections.