This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: VREGENZ pin connected to VSS that isn't supported

Part Number: TMS320F28377S


Tool/software:

Dear expert, 

In our old DS, we didn't mention that the VREGENZ isn't supported. 

SPRS881C:

SPRS881D:

SPRS881I:

If the user has already connected the pin to VSS, will there be any issue coming? 

Best Regards,

Eric Chen

  • Hi Eric,

    Does the customer also have an external voltage regulator, or are they solely relying on the internal voltage regulator?

    Thanks,

    Ben Collier

  • Dear Ben, 

    They rely on the internal one, but actually didn't encounter any issue yet. 

    But is there any potential risk that user should take care of? 

    Or can we have more details about how the internal voltage regulator will work when the VREGENZ pull to VSS? 

    I think the VREGENZ shouldn't have any function because the feature isn't supported on F28377.

    Best Regards,

    Eric Chen

  • Hi Eric,

    The problem is that the internal regulator cannot supply this maximum of 400 mA 

    It is possible that the customer's application never puts a load on the CPUs that require this much current consumption, but our recommendation has to be that the customer uses an external voltage regulator for Vdd. We cannot guarantee reliable operation with internal voltage regulator.

    Best Regards,

    Ben Collier