This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039: TMS320F280039:MCAN Busoff Recorvery Error

Part Number: TMS320F280039


Tool/software:

HI,

    When we were conducting the Busoff test of the MCAN module (the way to trigger busoff is to continuously short-circuit CAN-H and CAN-L), after reinitializing MCAN, the application layer attempted to send a message. Due to the continuous short-circuiting of CAN-H and CAN-L, it would enter busoff again. However, there may occasionally be another busoff interruption after an interval of approximately 2.8 ms, as shown in the last descending section of the blue line in the following figure. What could be the reason for this?