Part Number: TMS320F28377D
Tool/software:
Hi Expert
Customer has one debug support need: they need to debug APP code in Boot + APP project.
Customer's project structure is:
- customer boot located at 0x80000 to 0x86000,
- app code located at the flash behind 0x86000,
- Customer boot and app code are 2 separate projects.
Now customer want to only debug APP code but keep the boot code. they see the variables are all "0" shown in the Expressions window when they do this kind of debug.
Could you please kindly help to see whether there is a workaround to help customer realize this debug?
Thanks
Joe